Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Are the iSW range of Din rail mounted switches suitable for Isolation?

Yes, the iSW range of switches 20 to 125A are suitable for Isolation and compliant with BS EN 60947-3.
These devices are Switch-Disconnectors therefore they have the functions of

  • Isolation - when in the “Open” position the isolation at a defined withstand voltage is assured between the open contacts of the main circuit of the switchgear.
  • Load Switching - they are able to open and lose circuits under load

These two functions are defined in the standard IEC 60947

Schneider Electric Ireland
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
  • Help and Contact Centre