Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
sea9de24 Enclosure internal drawings and dimension needs to know clearance around din rail

Please find attached a simplified drawing of SEA9DE24 Enclosure inside with iC60H RCBO (similar dimension than C60H RCBO) on the DIN rail.

You can see that the clearance distance between the bottom side of the RCBO and the bottom side of the enclosure is 58mm.

You can find dimensions and CAD documents on our website se.com, please use the following link https://www.se.com/uk/en/product/SEA9DE24/acti9-isobar-a---din-rail-enclosure---12-ways---steel/

cable entry

Knock-out 25 mm (top and bottom)

Knock-out 25 mm (rear)

Knock-out 25 mm (side)

height

300 mm

width

345 mm

depth

117 mm

Schneider Electric Ireland

Attachment(s)
sea9de24_with_rcbo.pdf [175.56 KB]
Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: