Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the part number for ATV320*****WS potentiometer complete with potentiometer and switch?

ATV320*****WS -----  this product came with the Vario main switch disconnector already fitted as per part code.

To make this a fully stand alone unit with the isolator . Start / stop switch and potentiometer you can add:  Potentiometer XB5AD912R4K7, the toggle switch ZB5AD3  (3 position stay put toggle switch) and ZB5AZ103, which is a contact block with 2 n/o contacts.

Or the item can be ordered as the ATV320*****ZH28 which would come completely assembled for a stand alone unit, fitted with the isolator start stop switch and the potentiometer.

Schneider Electric Ireland