Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to read energy consumption and peak KVA through modbus communications on power meter METSEPM5310.
1) For reading the Energy values from register 2700 onwards you have read the data in Float inverse format or Swapped float format.
Also If your reading with Base 1 then register will start from 2700 .
If your reading with Base 0 then register will start from 2699.
modbus table
modbus poll screenshot
2) For reading the KVA, read the data in Float inverse format or Swapped float format.
Also please take note Base 1 or Base 0 for reading the appropriate register.
modbus table
modbus poll
Once you have the Appropriate data type selected, base details selected and polling the right register according. Will give you the right values.

Schneider Electric Ireland

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: