Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the iC2000P+ twilight switch be used to switch contactors?

IC2000P+ can switch contactors. And is possible to switch the connected load by lux threshold. With a standard program (not extra program) you can define times when the switching according lux threshold is not considered, but light has programmed status (ON or OFF).

It is possible to connect up to 10 standard contactors with coil.
Note: "The IC2000P+ comes from an external supplier. Due to this they are not referring to Acti9 contactors or were tested with them. They were referring to standard contactors with coil."


Schneider Electric Ireland

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: