Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the Power Consumption for contactors used for capacitor banks LC1D*K*?

The LC1D*K range of contactor is based on Tesys D, with the LC1D50 and above being based on the D2 range (not everlink).

See below conversion for capacitor contactor to standard contactor. These are the bases that are used to make the capacitor contactors. You'll find the power consumption for a capacitor contactor on the data sheet for the equivalent base.

- LC1DFK = LC1D12
- LC1DGK = LC1D18
- LC1DLK = LC1D25
- LC1DMK = LC1D32
- LC1DPK = LC1D50
- LC1DTK = LC1D65
- LC1DWK = LC1D80

Always remember you need to add a voltage code to complete the part number. Common codes are B7 = 24Vac, BD = 24Vdc, F7 = 110Vac, and P7 = 230Vac. Just add the code to the end of the above reference to complete the part number e.g. LC1DFK with a 24Vac coil = LC1DFKB7. This goes for both standard and capacitor contactors.


E.g. LC1DFKB7 is based on LC1D12B7 frame. Power dissipation is given on the data sheet, see below. To find a data sheet, go to our website www.se.com/uk and type the contactor part number (the base contactor, LC1D12B7 in this case) into the search bar.

Power dissipation per pole0.36 W AC-3
1.56 W AC-1
0.36 W AC-3e

Schneider Electric Ireland