Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How is the neutral connection available in the Isobar P – Hybrid or Standalone Active distribution boards?

Neutral connection is made available for AFDD section only in Isobar P – Hybrid or Standalone Active distribution boards.

Note: The neutral link is always live (energized) once powered with electrical supply. Off-load disconnect switch function available only for Phase/Line on Active distribution boards.

Showcase the label & different sections of the pan assembly (zoom) & Neutral is not switching.
In these boards only 1P or 3P MCBs & 1P RCBOs can be mounted in the Top/PoNeo section & Acti9 Active in AFDD section as outgoers.

For regular Isobar P boards (A type & B type), with the use of SEA9NAXX we can use 1P&N outgoing breaker is used in Isobar type A board or B board. 3P&N outgoing breaker is used in Isobar type B board.
This product is not compatible for Isobar P – Hybrid or Standalone Active distribution board

Refer the video for installation Isobar P type A board -


List of available Distributed Neutral Link

Schneider Electric Ireland