How can we help you today?

Is the SDE adaptor (LV429451) for NSX 100-250 and NSX 400-630 Motor Mech, a spare part?

The SDE adaptor is included with NSX MT100-250 but you can order it separately as well part number LV429451. As for NSX 400-630 the SDE adaptor is not required.

SDE photo

This is an adapter part used with auxiliary contact SDE on Compact NSX 100/160/250 devices. This part is mandatory for control units TM, MA or Micrologic 2 if SDE contact is used.

Schneider Electric Ireland

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • General Terms of Business
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings