Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
When using Tesys T, can I use multiple control channels simultaneously?

The Tesys T (LTMR*) motor starter allows you to chose between 3 different control channels (terminal strip, HMI and Network) for each control source (Remote and Local), however, when in operation you can only use Remote OR Local control source at any one time. These control sources cannot be used simultaneously.

When configuring the unit on SoMove, you have to assign the Remote and Local control channels within the parameters list, "control tab", as below:

Local / Remote control channel Selection - Tesys T in SoMove

The options possible for Local and Remote controls are shown in the table below:

Control Channel Options - Tesys T

When in operation, the selection between Local and Remote will be done through input I.6, depending on the wiring mode. This is commonly done by using a Local-Remote selector switch wired to that input.

See user manual for further information: https://download.schneider-electric.com/files?p_Doc_Ref=DOCA0127EN&p_enDocType=User+guide&p_File_Name=DOCA0127EN-03_TeSys_T_Motor_Management_Controller_User_Guide.pdf

Schneider Electric Ireland