Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
which is the software to program the HMISCU range?

The Harmony SCU (former Magelis) range is an HMI controllers for simple machines with up to 16 Inputs and 10 Outputs including Ø 22 mm mounting system.

The part numbers of the HMISCU range are the following:

  • HMISCU6A5
  • HMISCU8A5
  • HMISCU6B5
  • HMISCU8B5

For further information about this range please check the catalog:

https://download.schneider-electric.com/files?p_Doc_Ref=DIA5ED2130505EN

The software to program the HMISCU range is EcoStruxure Machine Expert (former SoMachine).

The design of the HMI part is done with Vijeo Designer but it comes with the installation of EcoStruxure Machine Expert (if it is selected).

In order to program the HMISCU range a license is mandatory to be able to use Vijeo Designer after the trial version of the EcoStruxure Machine Expert.

In order to install this software you need to download "Schneider Electric Software Installer" from the next link:

https://download.schneider-electric.com/files?p_Archive_Name=ESEMACS10_INSTALLER.zip&p_enDocType=Software - Release&p_Doc_Ref=ESEMACS10_INSTALLER

Then you should be able to install EcoStruxure Machine Expert.

The software EcoStruxure Machine Expert has a Free version after the 42 days trial, please check pages 14 and 16 for more information for the free version limitations:

https://download.schneider-electric.com/files?p_Doc_Ref=DIA3ED2180701EN

The user that wants to use this software needs to have an account in our License Portal in order to register the software:

https://www.se.com/ww/sites/corporate/en/support/software-licensing/user-login

In the past the software was SoMachine and the latest version of this software was the SoMachine V4.3 SP2.

The reference for SoMachine is the SOMNACS43:

https://www.se.com/ww/en/product/SOMNACS43/somachine-software-v4-3-usb-drive-format/

In order to program the HMISCU range you can use a miniUSB cable (TCSXCNAMUM3P or BMXXCAUSBH018) or an ethernet cable.

Schneider Electric Ireland