Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which are the compatible connectors for the BMXDDO3202K?

The BMXDDO3202K needs a connector "One 40-way connector" for the 32 outputs:

X80 module

So we can use the:

•BMXFCW303 (One 40-way connector and two ends with color coded flying leads - 3 meters)

•BMXFCW503 (One 40-way connector and two ends with color coded flying leads - 5 meters)

•BMXFCW1003 (One 40-way connector and two ends with color coded flying leads - 10 meters)

If we want to use a Modicon Telefast ABE7 sub-bases with our Digital Output module then we can use the preassembled cordsets :

•BMXFCC053 ( One 40-way connector and two HE 10 connectors - 0.5 meters)

•BMXFCC103 ( One 40-way connector and two HE 10 connectors - 1 meters)

•BMXFCC203 ( One 40-way connector and two HE 10 connectors - 2 meters)

•BMXFCC303 ( One 40-way connector and two HE 10 connectors - 3 meters)

•BMXFCC503 ( One 40-way connector and two HE 10 connectors - 5 meters)

•BMXFCC1003 ( One 40-way connector and two HE 10 connectors - 10 meters)



In order to select the right  Telefast Pre-wired system please check the catalog for the Modicon ABE7 / ABE9

Schneider Electric Ireland

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: