Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which are the compatible connectors for the BMXDDI3232 ?

The BMXDDI3232 needs a connector "40-way caged or spring-type removable terminal block" for the 32 inputs:

X80 module

So we can use the:

•BMXFTB4000 (Caged-type removal terminal block).

•BMXFTB4020 (Spring-type removal terminal block).

Schneider Electric Ireland

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: