Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Which is the software for the "Discovery" packs SR3PACK (modular) and SR2PACK (compact) ?

The software to program the Zelio Smart Relay (SR2 or SR3 range) is the ZelioSoft2.

The latest version available is the ZelioSoft2 v5.4.2.2

Zelio Soft | Schneider Electric UK

In order to download or upload the program from Zelio we need to use the programming cable SR2USB01:

SR2USB01 - USB PC connecting cable - for smart relay Zelio Logic - 3 m | Schneider Electric UK

The SR2USB01 is not a standard cable. In case the drivers for the SR2USB01 are not installed in your laptop when you installed the software you can download it from the next link:

Driver for new USB-serial cable W7/8.1/10 (manufactured from week 1739) | Schneider Electric

The software is free to use, the customer needs to have an account in our License Portal in order to register the ZelioSoft2:

SWL Web Portal | Log In

In Zelio Smart relay we can have up 40 I/Os if you need more I/Os you will probably needs to take a look in other family range (Modicon M221).

For more information about our PLCs please access to:

Digi-Cat - Homepage

Schneider Electric Ireland