Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the tightening torque settings for the earth bolts in the Acti 9 distribution boards?
The main earth bolt (provided as a kit, using M8 hardware) should be tightened to 8.0Nm, this value is printed on the auto-bag.

The main earth terminal situated at the up of the board and using an  M7 x 15 combi head screw should be tightened to 3.5Nm.

Schneider Electric Ireland

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: