Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can the 3-pole MCCBs in the ComPacT NSXm offer be used in a single phase system?
Yes, the ComPacT NSXm MCCBs can be used for single phase systems.

Be advised the tripping curves for the NSXm MCCBs are advised if loaded three phase as standard. If loading a single phase system onto them the thermal protection managed by a bimetallic strip will trip slower than when 3 phases are loaded as represented on the curve.

See extract from catalogue:
TMD Extract

Schneider Electric Ireland

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: