How to Export logs on PM8000 range of meters
thank you for the enquiry please install ION setup this can be done through that software follow below
· Connect the meter to ION setup
· Click the meter name and then setup assistant
From this option, user able to change the interval needs.
Go to ION Setup and Click Setup Assistant, select Reports. There are two tabs, Meter Info and Data Collection. With Meter Info, User can export the Revenue Log, Energy Demand Log and Event Log, along with the meter configuration if that is desired for your records. User can select the number of records or a date range for data, and once the data is displayed, Users having the option to Save As file type options include CSV, TXT, PRN, XML and HHF.
The memory size available in PM8000 for data logging is 512 Mbytes. PM8000 series meter default logging framework which is configured to record data and events at pre-defined intervals or conditions:
The PM8000 series meter can support up to 50 data logs (data recorders) which can each record up to 16 different parameters.
Further details are available in Technical data sheet where customer can refer to it.
Related links:
The latest version of ION Setup can be downloaded from the link below.
https://www.se.com/in/en/download/document/ION_Setup_Latest_Release/
PM8000 User Manual:
https://www.se.com/in/en/download/document/7EN02-0336/
Released for: Schneider Electric Ireland