What is the Pinout wiring diagram of the cable XBT-Z9681 / XBT-Z968?
In order to connect a TSX Nano, TSX Micro or a TSX Premium to an older HMI Magelis (now we use Harmony) we need an specific cable to connect the Mini DIN 8-pin male of the programming port of the PLC to the SUB-D 25-pin male of the HMI.
The required cable could be the XBT-Z968 (8.2 ft / 2.5 meters) or the XBT-Z9681 (8.2 ft / 2.5 meters).
Below the pinout:
----------------
Note
Both XBT-Z968 (8.2 ft / 2.5 meters) & the XBT-Z9681 (8.2 ft / 2.5 meters) are now Discontinued without Replacement
Released for: Schneider Electric Ireland