Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Can I use a GSM modem with the Powerlogic PM5000 and IEM meters?
Unfortunately it is not possible to use a GSM modem to communicate with the Powerlogic PM5000 and IEM meters. You will need to follow the communicating wiring instructions for the product. For example, the A9MEM2455 and METSEPM5111 meters can only communicate using the RS485 port.

Schneider Electric Ireland

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: