How can we help you today?

Compact NSX MCCB peak current limiting curve

The green line is linked to 60947-2 standard table 2 representing the asymmetrical prospective peak current according to prospective short circuit current without limiting effect.

This line represents what would be the peak current seen downstream the breaker for a prospective short circuit current (abscissa) if the breaker would not be a limiter (Utilization category A).

Circuit breaker utilization

Current Limiting

Current limiting curves

This line is defined in IEC60947-2 standard table 2.

ratio table

This information is only useful to see the effects of a current limiting breaker on the following points:

Longer service life

Schneider Electric Ireland
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
  • General Terms of Business
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings