Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What could be the impact of running close to MCB capacity

Overheating and tripping:
When an MCB operates close to its rated capacity, prolonged usage at or near its maximum load can lead to increased heat generation within the device. This can potentially cause overheating, which may lead to premature wear and tear of the MCB components. Additionally, operating at high loads for extended periods can increase the likelihood of the MCB tripping due to thermal overload.

Reduced Lifespan:
Continuous operation near the MCB's maximum capacity can shorten its operational lifespan. The increased thermal stress on the MCB components may contribute to degradation over time, reducing its reliability and longevity.

Voltage drop:
In cases of high load demand, operating the MCB close to its capacity can lead to voltage drop across the circuit. This can affect the performance of connected equipment, especially sensitive electronics, and may result in decreased efficiency or malfunctions.

Safety concerns:
Operating an MCB at or near its maximum capacity may compromise the safety margin of the electrical system. In the event of unexpected load fluctuations or transient overloads, the MCB may be less able to provide the necessary protection.

To mitigate these potential impacts, it's advisable to size the MCB appropriately based on the load requirements of the circuit.

Schneider Electric Ireland

Explore more
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
  • Products Documentation
  • Software Downloads
  • Product Selector
  • Product Substitution and Replacement
  • Help and Contact Centre