Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to Achieve Anti-pumping on NW Circuit breakers

"In the event of maintained opening and closing orders, the standard mechanism provides an anti-pumping function by blocking the main contacts in open position. Anti-pumping function. After fault tripping or intentional opening using the manual or electrical controls, the closing order must first be discontinued, then reactivated to close the circuit breaker"

https://download.schneider-electric.com/files?p_enDocType=Catalog&p_File_Name=LVPED208008EN.pdf&p_Doc_Ref=LVPED208008EN

You can achieve the same process in the NSX range. This could be done using MN or MX.

Anti Pump via MX or MN

Schneider Electric Ireland