Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
What is the reference for the Vigi cable for the MasterPact ACB rectangular sensors?

The reference which can be used is code 47090. See link to datasheet below.

47090 - Vigi cables or external voltage cable - for Masterpact NT, NW | Schneider Electric UK

This is used on sensors such as LV833574SP and 33573.

Schneider Electric Ireland

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: