Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
Where can I find details for Tesys Contactors switching DC loads (as well as other specific applications)?

You can find this detail in our motor control and protection catalogue, specifically chapter A5. Refer to the section on utilisation categories, specifically the pages titled "Contactors for utilisation categories DC-1 to DC-5 ". In the attached example, it's pages A5/64-A5/67.

You can find chapter A5 in the Tesys Motor Starter catalogue.

  1. www.se.com/uk
  2. Type "Tesys" into the search bar
  3. Look under documents, catalogues and brochures, for the Tesys Catalog. Here is a link to the 2025 version (latest at the time of writing).

Link: https://www.se.com/uk/en/download/document/MKTED210011EN/

This chapter also contains information regarding type 1 and type 2 coordination, selection based on specific utilisation categories (In the case of DC, refer to DC1-DC5 selection tables), and selection based on specific applications such as heating, 3 phase transformers and capacitor switching.

Schneider Electric Ireland

Attachment(s)
A5 - Coordination and standards_P_EN (dgcat).pdf [2.71 MB]