Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
		
How can we help you today?
How to create a part number for the ComPacT NSX new generation of circuit breaker frames?
Issue
Users need guidance on how to construct a valid part number for the ComPacT NSX new generation of circuit breaker frames based on identifiable segments.

Resolution
The ComPacT NSX new generation part numbers are made up of identifiable segments. Each segment corresponds to a specific characteristic of the circuit breaker. By combining these segments, you can create a part number that matches your required specifications.

Example Part Number:
C10F3

Explanation of Segments:

  • C – ComPacT NSX series identifier
  • 10 – Frame size (e.g., 100A frame)
  • F – Breaking capacity (e.g., F = standard breaking capacity)
  • 3 – Number of poles (e.g., 3 poles)

General Structure:
[Series][Frame Size][Breaking Capacity][Poles]

SeriesFrame Size (MCCB Current Rating)Breaking Capacity (KA Rating)Number of poles
C100A = 1036KA = F3 Pole = 3
160A = 1650KA = N4 Pole = 4
250A = 2570KA = H
400A = 4075KA = HB1
630A = 63100KA = S
150KA = L
200KA = R

References

Schneider Electric Ireland

Explore more
Product:
Range:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product: