How can we help you today?

What is the output voltage (AC or DC) of the time delay relay for the MN Undervoltage release for Compact NSX Range?

The output voltage type of the delay unit for MN Undervoltage for Compact NSX range is "DC"

Compact NSXtable

Refer the below table for the delay unit and associated MN Undervoltage release for Compact NSX range

part numbers


You can see all the delay unit associated MN Undervoltage release coils are rated for DC voltage.

For Example - delay unit part number "33682" has input (control circuit voltage) of 200-250 V AC or DC but the output is 250V DC which will connect to 250V DC MN Coil part number "LV429414"

Schneider Electric Ireland

Explore more
Product:
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Product:
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
  • General Terms of Business
  • Privacy Policy
  • Cookie Notice
  • Terms of use
  • Change your cookie settings