Discover how SpaceLogic KNX Push Button Interface, make possible to keep conventional wiring devices and bring them into the KNX system. It can be used also to bring potential-free contacts and analog temperature sensor, into the KNX system. This video presents the available Push Button Interfaces and their features. It’s also highlighting their benefits at each step of a project: - Planning the KNX project - Installation - Commissioning
Date:
Apr 10 2025|Type:
How to video
Languages:
English|Version:
1.0
Subtype: Function and application, Installation details, System design
Document Reference:
knxpbinterfaceEN
The documentation available online is generally the latest version. Files