המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How can I utilize a user built keypad as an input for a data display in Vijeo Designer?

Issue:
Utilizing the user built keypad as an input for a data display in Vijeo Designer


Product Line:
Vijeo Designer


Resolution:
The following screenshot is a panel in Vijeo Designer with a data display and user built keypad.
keyboard Select the variable for the data display under the "General" tab.
Edit the data display to enable "Enable Input Mode" and disable the "Display Popup Keypad".
settings
This action will allow the user built keypad to be the input for the data display when you touch the data display on the XBTG terminal.

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)