המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How do you Access the Runtime Configuration from a Magelis XBTGT, HMIGTO, XBTGK and HMIGK using Vijeo Designer V6.2?

Article available in these languages: Spanish

Issue:
Need to change some system settings (IP address, date, and time) on the HMI but do not have Vijeo Designer to download the applicaton to it.

Product Line:
Vijeo Designer

Resolution:
The Runtime Configuration can be accessed a few different ways depending on how it is configured in the Vijeo Designer application:

1) Switch: Touch the switch set up with the Configuration system operation.

2) Top-Left Corner: Touch the top-left corner of the screen within ten seconds after the unit begins starting up.

3) Touch two corners successively: Touch successively the top left corner then the bottom right corner within half a second. The touch area is 50 dots by 50 dots. Vijeo Designer Runtime restarts and displays the Settings menu.

Here below is where the setting is set in the Vijeo Designer application. The property is called "To Configuration" and it is found in the Target's Property Inspector:
ToConfiguration