המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Where can I find custom built electrical drawings for enclosed drives and Soft Starters?

Issue:
Looking for custom build electrical drawings for enclosed drives and Soft Starters.

Product Line:
All Altivar and Altistart enclosed

Environment:
All

Cause:
Need custom drawings to assist with troubleshooting control circuit.

Resolution:
S-Flex, E-Flex, ATV660, and ATV960 units have some elementary drawings available in their respective installation documents.
Most enclosed drives are custom made and require a factory order number (drawing number) in order for the drawings to be pulled.
Call the Drives Product Support Group at 1 888 778 2733 and select option 2, then option 4, or email at drive.products.support@schneider-electric.com with the factory order number.

שניידר אלקטריק ישראל

קבצים מצורפים
E-Flex Instruction Manual 30072-451-51.pdf [5.87 MB]
S-Flex Manual 30072-451-83_06.pdf [6.67 MB]