המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the part number for the RFI filter grounding jumper for the ATV61HC11N4 Drives?
Issue:
Part number for the RFI filter grounding jumper for the ATV61HC11N4 Drives?

Product Line:
Altivar ATV61

Environment:
Only Frame size 9 ATV61 or ATV71 drives

Cause:
Customer removed and lost the RFI filter ground jumper and need to get a replacement.

Resolution:

The RFI jumper is included as part  of a Field Services only order kit part VY1A1303.

This part only can be ordered thru field services only.

I have attached a sheet of all of the parts that are included in the VY1A1303 kit.    The jumper part is not sold by its self.

This kit applies to Size 9 ATV61 and ATV71 drives only which are the  ATV61HC11N4, ATV61HD90N4 and ATV71HD90N4