המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How do I change the color of an image from the toolchest in Vijeo Designer?
Issue:
Looking for a way to change the colors of an image from the Toolchest of Vijeo Designer.

Product Line:
Vijeo Designer (all versions)

Resolution:
The images from the Toolchest are static and cannot be modified within Vijeo Designer. However, you could copy the image to a JPG or PNG file and modify it in a Graphical Editor like Adobe Photoshop or MS Paint.