המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Data Center Expert | What are the default credentials?
Issue:
Default credentials for StruxureWare Data Center Expert

Product Line
StruxureWare Data Center Expert (DCE)
- Basic Appliance (AP9465)
- Standard Appliance (AP9470)
- Enterprise Appliance (AP9475)
- Virtual Appliance (AP94VMACT)
StruxureWare Central (SWC)
InfraStruXure Central (ISXC)

Environment:
StruxureWare Data Center Expert (all versions)

Resolution:

Web Interface & Desktop Client
Username: apc
Password: apc

Viewing Network Settings
Username: apcinfo
Password: [user defined]
NOTE: Upon first setup using the apcsetup login, the password will be changed to a user defined password.

Configuring Network Settings
Username: apcsetup
Password: apcsetup    (Upon first logging in the password will be required to be changed)
Instructions can be found in knowledge base FA234266.

Root Operating System
Username: N/A
Password: N/A
For details see knowledge base FA222410.

NOTE: Please keep a secure record of this for future use.

If prompted, here are the initial configuration passwords.
Username: apcsetup
Password: apcsetup

Username: apcinfo
Password: apcinfo

Username: apcreset
Password: (7.9.2)= apc | (7.9.3 and above)= apcreset