המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Is it possible to use VW3 Sinus filter range with 3rd party variable speed drives - not Altivar ATV?
Schneider does not manufacture sinus filters, but buys them from supplier. All the combinations ATV+sinus filter that are mentioned in ATV catalog have been validated by performance test and therefore these combinations are guaranteed. Sinus filter is offered only as ATV accessory and their use with 3rd party drives is not guaranteed. The test must be done or managed by customer.