המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Can the ATV600 / ATV900 series drives stream live data from the data logger?
Issue:
How to get live data stream from ATV600/900.

Product Line:
ATV600 and ATV900 series drives.

Environment:
All models, All serial numbers.

Cause:
Customer wants to pull live data from the data logger on the drive

Resolution:
This function is not available on the drive through the data logger.  The data logger is designed to capture samples of data and make them available for download via SoMove.   For near real-time telemetry, connect a serial communication network such as Ethernet or Modbus TCP.  Many values are available to read in near real time.