המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
PME/PSE 8.x: Starting the Floating License Manager in 'Expert' mode

Issue
Starting the floating license manager in expert mode.

Product Line
Power Monitoring Expert 8.x

Power Monitoring Expert 9.x

PowerSCADA Expert 8.x

Environment
Floating License Manager

Cause
Modify and/or delete corrupted PME/PSE licenses.

Resolution
1. Create a shortcut of the 'FloatingLicenseManager.exe' file found at the following default directory:
C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\Floating License Manager

2. Right-click on the 'Floating License Manager' shortcut file and select 'Properties'.
Add 'expert' after the following entry in the Target parameter: "C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\Floating License Manager\FloatingLicenseManager.exe"
E.g. "C:\Program Files (x86)\Schneider Electric\Power Monitoring Expert\Floating License Manager\FloatingLicenseManager.exe" expert

Shortcut target path

3. Click 'OK' in the properties window to apply and save the changes.

Note: PME 2021 and later use the License Configuration Tool