המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to write to Modbus registers on an ION Meter and PM8000

Issue
Cannot write to the Modbus registers.

Product Line
ION Meters
PM8000

Environment
ION Frameworks

Cause
By default, the Security Options Modules (SOP1) Modbus Map Access setting is set to No.

Resolution
Change the SOP1 Modbus Map Access setting to yes:

  1. Open the meter inside of ION Setup.
  2. Ctrl + Click on the meter on the left side of the screen to open the advanced modules list.
  3. Open the Security Options Modules folder, and then open the Security Options 1 module.
  4. If prompted for a password, enter the front panel password (Default 0).
  5. Under the Setup Registers tab, Select the SOP1 Modbus Map Access option.
  6. Click Edit... and change the drop down from "No" to "Yes" and press OK.
  7. Select Send at the bottom of the window and the configuration settings will be saved.

The latest version of ION Setup can be downloaded at the link below.
ION Setup Software

For instructions on how to add an Ethernet device to ION Setup please refer to page 47 in the ION Setup User Guide that can be obtained by visiting link below.
(Note: The latest version of ION Setup software may not be up-to-date from the link below)
ION Setup Software and Documentation