המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Configuration Manager Tool 2020 - Unable to Write to System - PME Portuguese Language
Issue
"Write to System" is grayed out when trying to write an archive from a "PME 2020 - language Portuguese" into a new "PME 2020 - language Portuguese" - regardless if it is distributed or standalone.

Product Line
Power Monitoring Expert 2020

Environment
Configuration Manager Tool 2020 (CM Tool 2020) - System Migration PME 2020 to PME 2020

Cause
The registry CultureInfoName in a PME system for Portuguese version is set to "pt-BR" however CMTool file that reads the supported versions is using "pt", hence the tool cannot recognize this as a supported path.

Resolution
  1. Open Configuration Manager Tool 2020 > bin > SupportedVersions.xml in a notepad (make a copy of this file just for safety).
  2. Search for Languages="pt"
  3. You will find 4 lines:
    • Line 189:       <From Version="9.1" InstallationTypes="Distributed" Languages="pt" Editions="" />
    • Line 190:       <To Version="9.1" InstallationTypes="Distributed" Languages="pt" Editions="" />
    • Line 237:       <From Version="9.1" InstallationTypes="Standalone,Distributed" Languages="pt" Editions="" />
    • Line 238:       <To Version="9.1" InstallationTypes="Standalone,Distributed" Languages="pt" Editions="" />
  4. Replace it for Languages="pt-BR"
  5. Save it.