המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to download pdf from Electrical Organisation tab in EPB Rapsody software using dopdf tool
Step1: Download the dopdf tool from internet or also you can use the link : https://dopdf.soft112.com/quick-download.html to download dopdf executable file.
Step2: Install the dopdf tool.
Step3: Now you can go to Electrical Organisation tab in Rapsody software and press Ctrl+P or use the print tool from right side of the software as shown below to print the diagram.


Step4: A print window will open, in Name field you can select dopdf from drop down as shown in screenshot below and click OK.

Step5: Select the directory/folder where you want to save the pdf and name the file using Browse button as shown below and then click OK.

Step6: Now you can navigate to the directory/folder where you have saved the pdf and you should be able to view it.