המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Why "PRJ_VERS" EFB created with a name “PROJECT” inside a DFB "CM_EXCHANGE" is omitted at application import from Control Expert V14.1 to Control Expert v15 SP1 ?
Issue:
A project is created in CE V14.1 in which EFB “PRJ_VERS” is created with a name “PROJECT” inside a DFB “CM_EXCHANGE” (refer the screenshot below)
1.png
When this project is exported and opened in Control Expert V15 SP1, this EFB “PRJ_VERS” is deleted (refer the screenshot below) and project couldn’t be rebuild in CE V15 SP1
2.png
Solution:
There is a name conflict with subfield "PROJECT" of type PRJ_VERSION inside DFB CM_EXCHANGE. We cannot create such instance normally, since "PROJECT" is a reserved namespace.
User should rename the variable before the import or create a new variable. Instead of naming "PROJECT" to PRJ_VERS, use other name.
If EFB “PRJ_VERS” is renamed to any other name except “PROJECT” (for example “test”), this EFB will remain in CE V15 SP1 after the import. (refer screenshots below)
3.png
After import in CE V15 SP1:
4.png