המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Why after enter a Runtime license in EcoStruxure Machine SCADA Expert, the BuildTime trial period is expired?
In some cases, when a customer enter a valid Runtime License in his computer, The 40h trial period for Buildtime is getting lost.
In case the customer need to make some minor modification on the project, it can be helpful to have the trial period still available
The goal of this FAQ is to explain how to recover the 40h of evaluation mode

This article is applicable for EcoStruxure Machine SCADA Expert, all version

To recover the evaluation mode after enter a runtime license, it will depend of the kind of Runtime license (Hardkey or softkey)
  • If the Runtime license is Hardkey, launch "EcoStruxure Machine SCADA Expert 2020 Register" & select Softkey
  • If the Runtime license is Softkey, launch "EcoStruxure Machine SCADA Expert 2020 Register" & select Hardkey