המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How can I automatically resize my project panels and objects in Vijeo Designer?

Issue:
How can I automatically resize my panels and objects in Vijeo Designer when switching HMI targets?

Product Line:
Vijeo Designer v6.2

Resolution:
You can only automatically resize your panels and objects if you are going to a bigger screen resolution. If downgrading the resolution size, you will need to manually resize the objects accordingly.

There is a checkbox to check if you want it sized up automatically:
size up project

Notice you are not presented with this option when going to a lower resolution HMI:
downsize project

If this FAQ did not solve your issue, you can chat with us at chat with us or e-mail us at customer.services@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)

שניידר אלקטריק ישראל

גלה עוד
מוצר:
גלה עוד
מוצר: