המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Is the EVlink Pro AC energy measurement MID certified ?

Article available in these languages: Thai

There is a MID Energy Meter embedded in EVlink Pro AC chargers that have the letter M in the reference. The energy measurement for these chargers is MID certified.
For the other EVlink Pro AC references, the energy measurement is performed by an electronic card inside the charging station. The measurement accuracy is 1% but it is not MID certified. It is also possible to connect an external Energy Meter (MID or not MID) via Ethernet or RS485.
MID Energy Meter references: A9MEM2155, A9MEM3155.
Energy Meter references (not MID): A9MEM2150, A9MEM3150.