המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
ATV320 parameters transfer using simple loader.
Issue:
What is the procedure for uploading and downloading  the parameters to an ATV320 from the Simple Loader tool?

Product Line:
ATV320

Environment:
All

Cause:
NA

Resolution:
The uploading and downloading takes about about 34 seconds to complete.
Pressing any button will initiate the process, but once blinking, should be let go. During the download to the drive, there is a momentary LED blink, followed by a 2nd blinking period of a few seconds. The loader should not be disturbed during this time.

For erasing the Simple Loader, depressing both buttons until the loader starts blinking red is all that is required, and this process completes right away.