המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Why are the REAL data type variables data not showing correctly in Vijeo Designer when communicating to a M340 PLC?
Issue:
REAL data type variables data not showing correctly in Vijeo Designer when communicating to a M340 PLC.


Product Line:
Vijeo Designer, M340


Resolution:
The REAL data type variables may not show correctly due to word order not set correctly in Vijeo Designer. When the HMI is communicating to an M340 PLC the double word order must be "Low word first". To change the word order, expand the I/O manager in the navigator and double click on the equipment.

imagew

Ensure that the Double Word word order is set to "Low word first"
image2