המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Why are the REAL data type variables data not showing correctly in Vijeo Designer when communicating to a Unity Quantum PLC?

Issue:
REAL data type variables data not showing correctly in Vijeo Designer when communicating to a Unity Quantum PLC


Product Line:
Vijeo Designer, Quantum PLC


Resolution:
The REAL data type variables may not show correctly due to word order not set correctly in Vijeo Designer. When the HMI is communicating to an Unity Quantum PLC the double word order must be "High word first". To change the word order, expand the I/O manager in the navigator and double click on the equipment.

image3

Next, ensure that the Double Word word order is set to "High word first"
image4