המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Connecting Unity Loader to an M340 fails with TCP/IP (there are no issues connecting with Control Expert).
If you cannot connect to an M340 with the Unity Loader through TCP/IP and there are no issues connecting with Control Expert, it is recommended to check the firewall settings to ensure that Unity Loader is not being blocked.

There have been reported issues where some firewalls (i.e., Firewall Timed Group, etc. ) are blocking Unity Loader from accessing the M340 over TCP/IP.