המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
Why the presence of IO Scanning table and the absence of NOE module in the hardware configuration of an M340 project resulting from the conversion of a Premium TSXP572634M project with UMAC V3.2.9?

Issue

In UMAC version 3.2.9, rules are defined in the UMAC analysis operation to check and see if the Premium project is a good candidate for upgrading to M340.

One of the rules is to check if the Premium processor has a local Ethernet port with I/O scanning capabilities. If so, UMAC won't do the scan. This is done because the M340 does not have IO scanner capabilities on its native Ethernet port.

With UMAC 3.2.9 TSXP572634M was listed on the good candidates list even if it is not the case.

Thus, the existing IO Scanner table in the TSXP572634 Premium project will be converted to the M340 project but UMAC will not add a NOE module to the hardware configuration.

Product Line

TSXP572634 Premium, M340

Environment

Windows 10 Pro Version 21H2, Unity M580 Application Converter Version 3.2.9 (Standard), EcoStruxure Control Expert V15.2 - 220711

Resolution

This is an issue that should be resolved to some extent in the next version of the UMAC tool.