המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
How to set up an ATV212 for dual ramp functionality?

Under main menu,

ACC and DEC will be the first set of ramp up and down times.

Set AU1 to 0 to disable auto ramp feature.

Under AUF, F---:

Set F500 (acc2) for second ramp up time based on frequency threshold (F505).

Set F501 (Dec2) for second ramp down time.

Ramp switching can also be accomplished based on a logic input trigger vs a hz value threshold.

“If this article does not answer your question, check out our FAQ database that has answers to more commonly asked questions:

Frequently Asked Questions - Schneider Electric (se.com)

If this FAQ did not solve your issue, you can call us at 1-888-778-2733 Option 2 and then 4 or e-mail us at drive.products.support@se.com to create a case with our Technical Support Team.

If you are not located in North America, please contact your local Customer Care Center for assistance:

Support | Schneider Electric Global (se.com)