המותגים שלנו

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
What is the handle force required to operate the handle of a PowerPacT H Frame circuit breaker?

Product Line: Molded Case Circuit Breaker

Resolution:
The following forces are required to operate the handle of PowerPacT H Frame circuit breaker:

ON - 14.8 lbs  (force required to close the breaker by pushing the handle from OFF to ON)
OFF - 16 lbs (force required to open the breaker by pushing the handle from ON to OFF)
RESET - 20.7 lbs (force required to reset the breaker after a trip by pushing the handle from TRIPPED to OFF)