המותגים שלנו

Impact-Company-Logo-English Black-01-177x54

ברוכים הבאים לאתר האינטרנט של שניידר אלקטריק

ברוכים הבאים לאתר שלנו.
		
איך נוכל לעזור לך היום?
NetBotz Downloaded sensor data in CSV file shows special characters
Issue:
NetBotz Downloaded sensor data in CSV file shows special characters

Product Line:
NetBotz

Environment:
NBRK0750
NBWL0755

Cause:
Netbotz allows the user to download CSVs, mainly the Temperature Sensor data CSV, the Rack Access CSV, and the Alarms CSV. When a customer opens a CSV downloaded from Netbotz in Excel, strange characters will sometimes appear.
A specific example is that Temperature Sensor data has a temperature degree symbol, which is replaced by random characters.
This is only a problem when opening a file in Excel.
Other apps like Numbers read the data normally. This is because Excel does not automatically recognize UTF-8, the format of the CSVs.
So, certain bytes in the text file are being read as the ANSI encoding in Excel.

Resolution:
Instead of double-clicking and opening the file directly in Excel, do the following:

Open Excel Go to “New” and create a blank workbook

Go to “Data” in the Excel app

Click the dropdown “Get Data (Power Query)”

Select “From Text (Legacy)”

Select the CSV, in this case the temperature sensor data CSV

The Text Import Wizard should automatically appear. Select the “Delimited” option

On the same screen, click on the “File origin” drop down menu. Select “Unicode (UTF-8)”. Click Next

In the “Delimiters” column, deselect “Tab” and select “Comma”

Click “Finish”. The data should default to the Existing sheet, with the formula =$A$1

The data should appear with no strange characters in the UTF-8 encoding.